Share this Job

CNC Programmer 3rd Shift Shelby (NC)

Apply now »
Apply now

Date: Jul 14, 2017

Location: Shelby, NC, US

Company: Greenheck Group

General Summary:

Enhance material utilization and support company production goals through the daily implementation and continuous improvement of CNC machine programs.

Principal Duties & Responsibilities: 

  • Provide daily programs for CNC production equipment (laser, plasma cutters, turret punch presses, press brakes, etc.).
  • Load CNC programs into the computer and select raw material options to be used.
  • Analyze material utilization and make improvements to the CNC programming to achieve desired improvements.
  • Use Enterprise Resource Planning systems to review and adjust for changes in parts requirements.
  • Make recommendations on raw material inventory levels based on the production schedule and anticipated material utilization.
  • Adjust existing programs to accommodate product redesigns or production changes.

Business Unit Specific Duties & Responsibilities: 

  • Run daily batch of CAD and press programs resolve issues in a timely manner.
  • Able to manually nest parts as needed resolve issues in a timely manner.
  • Understand and able to perform basic scheduling functions.
  • Track and evaluate material utilization opportunities within fabrication area.
  • Capable of achieving full understanding of equipment operating systems
  • Perform remote nesting as needed.  Will require learning multiple nesting platforms.
  • Determines sequence of operations within a program for continuous improvement in efficiency.

Job Qualifications:

  • Work requires extensive technical or specialized training such as that which would be acquired in the first two or three years of college or technical school.
  • Experience with one or more nesting and instructional equipment software such as Majestic Trunest, Radan Radbend, Salvagnini equipment software.
  • Operation experience with fabrication equipment – laser, brake press, turret punch press, etc. is a plus.
  • Experience with inventory management transactions within any ERP system such as SAP is a plus.


Nearest Major Market: Charlotte